Part Number: TPS65988DJ
Hello,
I have a customer who is interested in using the TPS65988DJ with Tapex Creek design,
Can firmware image for TPS65988DJ work with Dual port configuration when Port A is fully TBT3 and Port B is Charger Only?
Port A PD capability: Source Mode 15W and Sink Mode 5V/9V/15V@3A and 20V@4.25W
Port A should be supporting fully Thunderbolt 3 Spec and Fully Standard USB-C Spec (DisplayPort Alternate Mode, USB3.1 Gen 2, Multi function USB3.1 Gen 2 + AM, Thunderbolt 3 Alternate Mode + PCIe Data, Thunderbolt 3 PCIe data)
Port B PD capability: 5V/9V/15V@3A and 20V@5A
Thank you.