Recently I'm working on new board. On this board there is one LVDS transmitter SN75LVDS84ADGG to interface display signals.
As we are trying to reduce the input signals driving strength to SN75LVDS84ADGG from CPU for better system EMC performance, we slow down the rise/fall time of input clock and data (i.e. CLKIN and Dn to SN75LVDS84ADGG ).
Current the rise/fall time measured on CLKIN is 11ns/5ns, on the Dn line is about 5ns/5ns. These don’t meet 5ns requirement in the SN75LVDS84ADGG datasheet.
But the setup/hold time between Dn and fall-edge of CLKIN well meets the 3ns/1.5ns requirement in the SN75LVDS84ADGG datasheet
If our board provides slow rise/fall time input signals to SN75LVDS84ADGG but still meeting the setup and hold time requirement, will there be any risk ?