Part Number: HD3SS214
Hello,
I would like to correct my schematic. Please refer to the design picture below. The bottom part works via USB type C and the top part doesn't work. This is because I have AC coupling caps on AUX N/P lanes between the MXM card and H2/H1 AUXp/AUXn pins of HD3SS214I and PTN3360DBS needs DC coupling . If I replace the AC coupling caps with 0 ohms, the top circuit works but bottom won't work as TUSB1046AI-DCI needs AC coupling.
On the AUX P/N lines, is it okay to DC couple between MXM card and HD3SS214I and AC couple between HD3SS214I and TUSB1046AI-DCI? So the entire path from MXM card to HDMI via the level translator is DC coupled while through the USB C circuit is AC coupled.