Part Number: TMUXHS4212
Other Parts Discussed in Thread: TUSB321AI, , TUSB322, TUSB8020B
Dear All,
please can you confirm our statements and suggest answer to questions
Type-C Receptacle Pin-out

1) DFP mode, Host side, Type-C Receptacle ->confirmation
1a) if CC1 (pin A5) connected to CC1 of TUSB321AI and CC2 (pin B5) connected to CC2 TUSB321AI ->
and TX port connected to ( A0 TMUXHS4212 ) -> then (B0 TMUXHS4212) port is TX1 and connected to A2/A3, (C0 TMUXHS4212 ) port is TX2 and connected to B2/B3 ? (please confirm)
1b) if CC1 (pin A5) connected to CC2 of TUSB321AI and CC2 (pin B5) connected to CC1 TUSB321AI ->
and TX port connected to ( A0 TMUXHS4212 ) -> then (B0 TMUXHS4212) port is TX2 and connected to B2/b3, (C0 TMUXHS4212 ) port is TX1 and connected to A2/A3 ? (please confirm)
2) UFP mode, Device side, Type-C Receptacle ->confirmation
1a) if CC1 (pin A5) connected to CC1 of TUSB321AI and CC2 (pin B5) connected to CC2 TUSB321AI ->
and TX port connected to ( A0 TMUXHS4212 ) -> then (B0 TMUXHS4212) port is TX1 and connected to A2/A3, (C0 TMUXHS4212 ) port is TX2 and connected to B2/B3 ? (please confirm)
1b) if CC1 (pin A5) connected to CC2 of TUSB321AI and CC2 (pin B5) connected to CC1 TUSB321AI ->
and TX port connected to ( A0 TMUXHS4212 ) -> then (B0 TMUXHS4212) port is TX2 and connected to B2/b3, (C0 TMUXHS4212 ) port is TX1 and connected to A2/A3 ? (please confirm)
3) is it possible to change P/N like
TXp connected to A0p, TXn connected to A0n -> then Connect TXp1(A2) to B0p, TXn1(A3) to B0n, TXp2(B2) to C0n, TXn2(B3) to C0p ?
Type-C Plug Pin-out

4) UFP mode, Device side, Type-C plug question
what is the proper connection of TMUXHS4212 +TUSB321AI when Type-C plug connector is used on UFP device side regards to receptacle connector?
Best Regards,
David.