Part Number: ONET4201PA
Other Parts Discussed in Thread: OPA855, ONET8551T, LMH32401
Using the following two types of ICs,
I am trying to design an optical data receiving circuit that meets a communication rate of 1 Gbps.
・ OPA855
・ ONET4201PA
I am trying to connect an APD (avalanche photodiode) to an OPA855 in order to improve the reception sensitivity.
The following is a rough configuration.
Light receiving element (APD) ⇒ TIA (OPA855) ⇒ Limit / RSSI (ONET4201PA) ⇒ CDR ⇒ FPGA
The most ideal application is like the ONET8551T It is a functional composite type IC for optical fiber,
but the package type is There are only wafers / dies.
Must be selected by chip package.
Since the application example of OPA855 is not data communication, it is as described above.
I would like to know if it can be used for high-speed data communication of 1 Gbps.
If your IC has the optimum configuration to realize the above configuration,
Please also make a suggestion.