This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: FPD-Link Performance

Part Number: DS90UB936-Q1

Hello support member

Please tell me about the FPD-Link of DS90UB936-Q1.

Q1.
Is it able to receive for 1.3MP/60fps ?

Q2.
Is it able to receive the Channel0 for 1.3MP/60fps, the Channel1 for 1.3MP/30fps?

Best Regards,

  • Hello Mukku,

    Thank you for reaching out. I have a few questions before I can provide you an answer.

    What is the CSI-2 Lane speed?

    What video format are you using?

    What clock type are using?

    Best Regards,

    Shruti

  • Hello Shruti

    I'm sorry to late the reply.
    I could receive an answer from the customer.

    Q1. What is the CSI-2 Lane speed?

    A1. 400Mbps x 4Lane (384Mbps@24MHz REFCLK)

    Q2. What video format are you using?

    A2. 1280 x 480 (2400 x 556 including blanking) YUV422 8bit

    Q3. What clock type are using?

    A3.  REFCLK 24 MHz (uses the serializer in synchronous mode)

    My question

    Q1.
    Is it able to receive for 1.3MP/60fps ?

    Q2.
    Is it able to receive the Channel0 for 1.3MP/60fps, the Channel1 for 1.3MP/30fps?
    (I also wonder if it is able to set different frame rates on Channel0 and Channel1.)

    Best Regards,

  • Hello Mukku,

    Thank you for providing the details. 

    Q1.
    Is it able to receive for 1.3MP/60fps ? ---> Yes

    Q2.
    Is it able to receive the Channel0 for 1.3MP/60fps, the Channel1 for 1.3MP/30fps? ---> Yes

    Yes, you can set different frame rates on Channel0 and Channel1.

    Best Regards,

    Shruti