Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
We have one new project, that would use TI DSP(spiclk can reach 12.5M), which is without CAN FD a.
We promote TCAN4550-Q1 as SPI to CAN FD bridge transciver.
The limitation is, for F28034 DSP, the max SPI clock is 12.5MHz max.
Could you help check with 12.5M SPI clock, what’s the CAN FD max data rate could be ? And how to calculate or evaluate ?
Customer is expecting 5Mbps CAN FD, if TCAN4550 could not meet, do you have any other suggestions ?
I understand that the data rate from SPI to CAN FD is satisfied, but the speed from CAN FD to SPI depends on the maximum memory of a single CAN message and the minimum time between two CAN messages
Can you tell me if the SPIclk clock is set to 18M and CAN 5MHz are connected? Or SPICLK18M speed is just a hardware process limitation,
Thanks.