Other Parts Discussed in Thread: TUSB2E22
Hi Experts,
Good day. I came to this forum with reference to my previous post:
SN74AXCH1T45: Data rate query
Based on our interaction there with an experts, the client responded as follows:
"But the problem is we don't have any IP to support USB 2.0 or eUSB.
So I am using an external PHY IC which can support USB2.0.The output of the TUSB2E22 repeater needs to be interfaced with that ULPI IC.
Hence the ULPI IC is compactable for USB2.0 the voltage level is 3.3V.
Also, I need to support both USB2.0 and eUSB in the system."
I am attaching their block diagram for your reference. Hence, they're looking for that kind of device that can support 1.2V to 3.3V and up to 480Mbps rate. Any thoughts on this?
Thank you for your support.
Regards,
Archie A.