Part Number: SN65DPHY440SS
Other Parts Discussed in Thread: SN75DPHY440SS
Dear team
As shown in the figure below, the main board (A) and Camera Module board (B), the relative position length of the two sides is about 500mm due to the structure ID setting.
1. Is it suitable for ICs such as MIPI Retimer (SN65DPHY440SS/ SN75DPHY440SS) to extend the signal length?
2. If it is possible, Retimer is recommended to be placed on the B side?Or other??
3. In general, what is the maximum length of this type of Retimer?
Are there other more suitable feasible solutions for this relative length?

Many thanks
Denny