Part Number: DP83822I
Hello Team,
As per PHY Datasheet below are the Power up timing,

Query -:
1. Is it ok if RESET_N pin goes High before T1?
2. Is it ok if RESET_N pin goes High before VAVD/CT goes high?
Thanks and Regads,
Ramdas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
Hello Team,
As per PHY Datasheet below are the Power up timing,

Query -:
1. Is it ok if RESET_N pin goes High before T1?
2. Is it ok if RESET_N pin goes High before VAVD/CT goes high?
Thanks and Regads,
Ramdas
Hi Ramdas,
To answer your questions, it is okay if the RESET_N pin is pulled high before T1 (and therefore before VAVD). This does not mean the PHY is ready to go immediately (it still has to go though POR).
Sincerely,
Gerome
Hello Gerome San,
Thanks for your feedback.
I understood that T1 is VDDIO and VAVD supply ramp time and it is 100ms max.
Also, T3 - Hardware configuration latch-in time for power up is Typ. 200ms after RESET_N
So, total maximum time to access PHY after power ON is 300ms/
Is my understanding is correct?
Thanks and Regards,
Ramdas
Ramdas-San,
Worst case, it will be 400ms from power on (VDDIO ramp start to AVD ramp start at worst 100ms later to AVD ramp completed after 100ms to 200ms for T2).
Sincerely,
Gerome