Part Number: DS90UB947-Q1
Dear team,
For the LVDS data line layout, they need to be treated with equal length. Then for the LVDS data and clock, do they need to be treated with equal length?
Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB947-Q1
Dear team,
For the LVDS data line layout, they need to be treated with equal length. Then for the LVDS data and clock, do they need to be treated with equal length?
Thanks & Best Regards,
Sherry
Hi Sherry,
If they are within the same group, I would recommend to have the same length. Yes you would need to make them the same length.
Hope this helps. Let me know if you have any questions.
Aaron
Hi Aaron,
If they can't make the same length due to PCB limit, what is the max tolerance?
Thanks & Best Regards,
Sherry
Hi Aaron,
Could you please help give me the reply today? My customer is waiting for the reply and then finish their layout.
Thanks & Best Regards,
Sherry
Hi Sherry,
All lanes need to be matched especially the clock to data skew. Within its ports, the trace length of the data must be matched referenced to the clk. For example, if PORT1 is used CLK0 from PORT0 then all data signal from PORT1 must be matched to the clock of PORT0. The max tolerance is about 5 mil.
Hope this helps. Let me know if you have further questions.
Aaron
Hi Aaron,
Thanks for your reply!
Understand. The max tolerance between clk and data is 5 mil. The max tolerance between data and data is also 5 mil, right? If we need to add vias to achieve the matched length, is it ok?
Thanks & Best Regards,
Sherry
Hi Sherry,
This is high speed routing. I would suggest that you should avoid to use via unless you need to. If you use via, then you need to make sure there is a ground reference via as well for both P and N.
Aaron