Other Parts Discussed in Thread: TCAN1042H
Hello,
I want to use SN55HVD251 in an application where the CAN signals will be bundled in a connector with +25V and GND. This is a high-cycle connector in a very wet/dirty environment, so the design must assume that steady-state connections between +25V and either CAN signal, or GND and either CAN signal, or the CAN signals to each-other, are likely. The hardware must not suffer damage in these situations (of course the system need not continue to operate while the short is present...)
The SN55HVD251 datasheets specifies +/- 36V bus fault protection, which I assumed meant that it tolerated a steady-state short between CANH/CANL and +/-36V without damage. However, section 8.3.5 states:
"The SNx5HVD251 has a thermal shutdown feature that turns off the driver outputs when the junction temperature nears 165°C. This shutdown prevents catastrophic failure from bus shorts, but does not protect the circuit from possible damage. The user should strive to maintain recommended operating conditions and not exceed absolute-maximum ratings at all times. If an SNx5HVD251 is subjected to many, or long-duration faults that can put the device into thermal shutdown, it should be replaced."
What am I misunderstanding? The thermal shutdown section seems to indicate that the CANH/CANL pins can not withstand a +/-36V short because the driver will enter thermal shutdown and incur damage over time. I suspect I am misunderstanding the definition of one of these terms.
Thank you!