Part Number: DP83TD510E
Hello,
How much flexibility in the value used for the strap resistor? Would it be OK to use a 3.0K, 2.7K, 2.2K, 2.0K, 1.8K etc.?
Thanks,
Cyrus
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TD510E
Hello,
How much flexibility in the value used for the strap resistor? Would it be OK to use a 3.0K, 2.7K, 2.2K, 2.0K, 1.8K etc.?
Thanks,
Cyrus
Hi Cyrus,
Please refer to table 7-5 of the datasheet. You must use 2.49kOhms, 1% tolerant resistors.
Sincerely,
Gerome
Hello,
I did refer to table 7-5. It says, "IDEAL RESISTORS" which implies that other values may be used. Can you please double check this? Requiring different exact resistor values that are very close to the same value adds extra components to the BOM and drives product cost up. If I could use even a 2.2K or 2.7K instead it would be very helpful.
Thanks,
Cyrus
Hi Cyrus,
I understand where you are coming from. The value is important to be close to as this external resistor connection completes a voltage divider circuit. When the PHY boots up, it samples the strapping pins to see which mode it will be in per strapping pin (in this case, mode 0 or mode 1). By attaching a different resistor value than what is provided in the datasheet, the voltage on that node may be different than what the PHY is expecting, which may cause it to bootup in a different mode than what you intend it to be. This problem becomes more apparent in our other PHYs which have 4 level straps (therefore a tighter window to be in). We cannot guarantee intended operation if you deviate from these values.
Sincerely,
Gerome