Part Number: DP83822I
Other Parts Discussed in Thread: DP83TD510E
Hello,
I am connecting a DP83822IRHBR to a DP83TD510E back-to-back via the RMII interface.
The DP83822IRHBR datasheet says RBIAS requires a 4.87K to GND. How much flexibility is there in the resistor value? Can I use a 4.3K, 4.7K, 5.1K?
The DP83822IRHBR datasheet says the MDIO pin requires a 2.2K pull-up resistor. How much flexibility is there in the resistor value? Can I use a 3.0K, 2.7K, 2.49K, 1.8K?
Thanks,
Cyrus