Part Number: TDES954
Team,
my customer is using DS90UB954, but they may switch to TDES954. The datasheets have different wordings:
- DS90UB954: FPD-Link 3
- TDES954: V3Link
They are using DS90UB953 as the counterpart and fear that the TDES954 is not 100% compatible.
Is the temperature range really the only difference between DS90UB954 and TDES954?
Thanks!