Other Parts Discussed in Thread: DP83869
Hello Team
My customer used DP83869HMRGZR to replace DP83867IRRGZ and did a compliant design, please see below schematic, they use some NC resistor to jump some pin connections.
When using DP83867IRRGZ, it can communication normally, but in DP83869HMRGZR, they met packet loss issue when communication with external PC as well as in loopback test.
They short the RJ45 1,3 and 2,6, and set below register for the loopback test:
0x1F = 0x8000
0x31 = 0x10b0
0x00 = 0x2100
0x16 = 0x10
0x10 = 0x5008
0x1F = 0x4000
I asked them to dump the all register:
read 0x0000=0x1140. read 0x0001=0x796d. read 0x0002=0x2000. read 0x0003=0xa0f1. read 0x0004=0x01e1. read 0x0005=0xc1e1. read 0x0006=0x006f. read 0x0007=0x2001. read 0x0008=0x4000. read 0x0009=0x0000. read 0x000a=0x0000. read 0x000f=0xf000. read 0x0010=0x5048. read 0x0011=0x7c02. read 0x0012=0x0000. read 0x0013=0x1c40. read 0x0014=0x29c7. read 0x0015=0x0003. read 0x0016=0x0000. read 0x0017=0x01e1. read 0x0018=0x6150. read 0x0019=0x4444. read 0x001a=0x0002. read 0x001e=0x0012. read 0x001f=0x0000. read 0x0025=0x0480. read 0x002c=0x141f. read 0x002d=0x0000. read 0x002e=0x0221. read 0x0031=0x10b0. read 0x0032=0x00d0. read 0x0033=0x0000. read 0x0037=0x0000. read 0x0039=0x0000. read 0x003a=0x0000. read 0x0043=0x07a0. read 0x004f=0x0200. read 0x006e=0x1020. read 0x0086=0x0377. read 0x0134=0x1000. read 0x0135=0x0000. read 0x0170=0x0c0f. read 0x0180=0x0752. read 0x0181=0xc850. read 0x0182=0x5326. read 0x0183=0xa01e. read 0x0184=0xe976. read 0x0185=0x19cf. read 0x0190=0x0000. read 0x0191=0x0000. read 0x0192=0x0000. read 0x0193=0x0000. read 0x0194=0x0000. read 0x0195=0x0000. read 0x0196=0x0000. read 0x0197=0x0000. read 0x0198=0x0000. read 0x0199=0x0000. read 0x01a4=0x0000. read 0x01a5=0x0000. read 0x01a6=0x0000. read 0x01df=0x0000. read 0x01e0=0x417a. read 0x0c00=0x0140. read 0x0c01=0x6149. read 0x0c02=0x2000. read 0x0c03=0xa0f1. read 0x0c04=0x0020. read 0x0c05=0x0000. read 0x0c06=0x0000. read 0x0c07=0x2001. read 0x0c08=0x0000. read 0x0c18=0x01ff. read 0x0c19=0x0010.
Can you please kindly help to see any potential root cause we can find? Thanks.
BR,
Rory