Part Number: TMDS181
Hi Team,
When TMDS181 measures the eye diagram, it is found that the EYE in the middle is pressed, but the output image is normal. Is there a solution?
The setting is strapping mode,
I2C_EN/PIN = Low; puts device into pin strap mode
PRE_SEL = 1/2 VCC
EQ_SEL = No Connect: Adaptive EQ; EQ_SEL = L: Fixed EQ at 7.5 dB at 3 GHz EQ_SEL = H: Fixed at 14 dB at 3 GHz also tried