Part Number: PCA9545A
Other Parts Discussed in Thread: TCA9543A, SN74LVC2G66
Hi team,
This is Andy, FAE of Inspur Group.
Inspur is using our PCA9545A at Server, and I have some question on how use PCA9545A, please help me check.
1. PCA9545A have four channels, if we just need 2 channels, how can I deal with the other unused channels?
2. PCA9545A also have voltage translation function, so I use 3V3 standby power rail powered PCA9545A VCC, Pull up Master and Slave channels SD0~SD2, but use another power rail 3V3 main pull up Slave SD3. The problem is 3V3 standby power on quickly, but 3V3 main will power on later, determined power-on time based on system requirements; During this time, the SD3 channel can be considered to be floating, so does PCA9545A support this application?, If we power PCA9545A like this, will the BMC appear abnormal when scanning PCA9545A?
If can't use like this, do you have some suggestions for this application to give our the customer, customer needs to use 3V3 main to pull up the SD3 channel, the purpose is to maintain the same power supply rail as the downstream device to avoid leakage current.
Thanks for your help and look forward your reply.
Best regards,
Andy Liu