Hello,
Our customer used DS90UB941+DS90UB948 for his application, there is only DSI0 input of DS90UB941 and dual link output, and the dual link connected one DS90UB948, and the 948 is dual OLDI output.
So the question is if the DS90UB948 support 1080p60 output?
My understanding is that if the FPD link side could support 1080p60, either single OLDI or dual OLDI output of DS90UB948 could support 1080p60, that is to say, the DSI0 input should also need support 1080p60(148.5Mhz), but the customer only use DSI0, the pixel clock could support 105MHz, so his this application is not feasible, what he should do is that he need to use dual DSI input, isn't it?
Best regards
Kailyn