Part Number: SN65LBC031
Hi Team,
What's the ESD performance of SN65LBC031DRG4?
Thank you!
Marc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Marc,
Looks like this part was never qualified for any ESD protection standards, or else it would be listed in the datasheet. Given that this is quite an old part (1998), this doesn't surprise me.
If you are concerned about ESD requirements, I would recommend external ESD protection circuitry for the device.
This device is fully protected against battery short circuits and specific electrical transients that can occur on the bus lines.

It also features thermal shutdown circuitry that disables the output drivers when the device dissipates too much power.
Regards,
Tyler