Part Number: TPS65988DK
Other Parts Discussed in Thread: TPS65988DJ
Hi all,
is the TPS65988DK useable as simple PD controller or have i use the DH variant of it? (i know it is asked many times but for me there is no clear answer...)
I only need the following:
- 2 ports, one SRC, one SNK.
- SRC has to use DRS because its UFP
- SRC should have at least two power profiles 5V and 9V
- SNK should request up to 9V
- BC1.2 is NOT needed
- Thunderbolt is NOT needed
- Displayport is NOT needed
if it is not possible to use the DK for this purpose i will accept this. But maybe there is a better answer than "it is for TBT or USB4".
thanks
best regards
philipp