Part Number: TSER953
Other Parts Discussed in Thread: TDES954
Question related to system capabilities:
Could two independent (but synchronized) 800x800 single-lane MIPI streams (one from each TSER953) to be bridged into a dual lane 1600x800 MIPI stream by the TDES954 (i.e. a single video stream with a single MIPI clock and two data lines, not two independent MIPI streams with independent clock and data lines). Ultimately could we connect the MIPI data to a Cypress EZ-USB CX3, which will then convert the MIPI data to a USB 3 video class stream. Done properly, I want to see a 1600x800 video on my monitor, with the left half of the video being one camera, and the right half being the other camera.