Part Number: TUSB8020B-Q1
Other Parts Discussed in Thread: TUSB8020B
Hi,
Currently we have issue whereby the host is not able to detect the TUSB8020B hub. We already check the connection:
- power up sequence is correct - 3.3V up before 1.1V
- USB_VBUS input 0.49V
- 24MHZ crystal input available. May i know what is the required input level? Xi is currently measured to be Vp-p 1.56V.
- SMBUSZ is NC. Measured to be 3.22V on pin.
- Reset pin is toggled after the supply is up per the spec.
May i know what other pin setting that may impact the host enumeration?
Thanks.