Part Number: TSU6111A
Hi,expert:
When I used TUS6111ARSVR chip to complete the usB-to-UART function design of my hardware control board, I found that when I inserted the USB cable into my computer, the computer could not connect with the control board.TSU6111ARSVR chip does not realize automatic detection (This document mentions automatic detection function:www.ti.com/.../tsu6111a.pdf )and connected function.Note: The main chip of my control board is F280049C.Please help confirm and answer the following questions:
1. Whether the hardware circuit design of my USB-to-UART function is correct;

2. Is it necessary to configure 150K impedance to realize automatic detection function?Can I do this by connecting two resistors of 75K in series?
Best Regards
Johnson Alanl