Other Parts Discussed in Thread: DS250DF230
Component number: DS250DF230
Hello TEAM.
When I configure the DS250DF230 chip according to the programming manual, the Configuration is as follows:

Channel A->A works, channel A->B does not.When I configure 0x96[2] to 1, channels A->A and A->B are both working, so, I have some questions:
1. I want to know the function of 0x96[2].
2. When configuring cross-channel, can only CONFIGURE A- >A,A- >B at the same time, but not A- >B at the same time?
Since I've tried many configuration methods and failed,
3. Can you elaborate on the meanings of 0x96[0]-0x96[3] and how I should use them

Best Regards,
zhangzhenq