Part Number: TUSB2036
Hello,
We are using TUSB2036VF in one of our applications where we are adding cellular and Wifi modules to the existing printer via USB.
We came across a few doubts :
1)Pin 21-Our cellular and wifi modules will be powered on by 3.3V and not with 5V, hub is used only for data transfer, so how to give overcurrent protection?
2)Pin 24- If we are not using 3rd port can we still configure the pin for 3 ports by making it low?
3)Datasheet recommends ferrite beads at the VCC pin it would be great if you suggest a part number of the ferrite bead
4)Should reset be permanently pulled up? because datasheet says reset must be asserted during power-up?