Hi Team,
I am using TCAN1044VDRQ1 in 2 wheeler cluster application.
Would like to get the schematic reviewed.
VCC is 5V, VIO is 3.3V.
Do i need to use Transistor for STB pin to meet VIO level? or can i connect the STB pin directly to Processor?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am using TCAN1044VDRQ1 in 2 wheeler cluster application.
Would like to get the schematic reviewed.
VCC is 5V, VIO is 3.3V.
Do i need to use Transistor for STB pin to meet VIO level? or can i connect the STB pin directly to Processor?

Hi Lakshmipriya,
While the input threshold for the STB pin will be set by the Vio level, the absolute maximum for this pin is still 6V. This means that a 5V input may still be used for STB when Vio is supplied with a lower voltage. For this schematic, the external level shifter is not necessary.
The rest of the schematic looks good. I don't have any changes to recommend. See my notes below.
Let me know if there are any questions or concerns regarding the design.
Regards,
Eric Schott