Part Number: SN65LVCP114
Hi Team,
my customer develops a Test Board:
The Test Board using FMC+ Connector with total amount of the 116 Single ended IOs
But our design comprise 184 pins.
Most of a pins are used for synchronous buses and can be multiplexed, one part can be transmitted on rising edge and second on the falling edge.
By doing so we can reduce the number of physical pins on board by two 184/2= 92 and solve our connector limitation.
We are currently looking for chip that can convert DDR data bus to two single clock edge busses and vice versa
Do you have an idea how to solve it?
Thanks
Jan