Part Number: DS90UB954-Q1
Hello support member
I received a question from a customer.
Please tell me about the configuration of the DS90UB954-Q1 Strap Pin.
I refer to "Table 2. Strap Configuration Mode Select" on page 30 of the datasheet(SNLS570B).
MODE No.0:RX MODE/CSI-2 nonsynchronous Back Channel)
Rlow:10.0K Ω.
Q1.
Is there any problem if it is connected directly to GND without 10.0K Ω?
Q2.
If there is a problem with direct connection to GND,
Please tell me what kind of problems there are.
Best Regards,