Part Number: DS90UH948-Q1
Other Parts Discussed in Thread: DS90UH947-Q1,
Hi Friends on the Interface group, I am investigating a design using the DS90UH948-Q1 DES and the DS90UH947-Q1 SER
I have a display with 1540x720 active area with a pclk of 75.41MHz
Both the mentioned devices provide OpenLDI ports on the output side and the input side respectively.
I need to pass a second OLDI channel through to the 947SER so effectively there are 2 selectable input sources,
My question is, has anyone come across any dedicatated device(even in a IP block) for such an application?
Each channel is either 10 lvds pairs(possibly 5 if the bandwidth allows).
Be interested to hear any thoughts on this.
Thanks
William