Part Number: TPS65988
Other Parts Discussed in Thread: TPS65987
I have a system that needs to be capable in a dead battery state and a normal state. the system is patched at boot by a micro over i2c , when the system is booted normally with a battery everything works. Then i can boot the system off dead battery and works as expected. Once i reboot back off battery and plug in the phone the phone goes through a pd hard reset (per a pd sniffer) and then takes about 30 seconds for it to react to the connection and then begin to work like it was in normal mode. I have tried clearing the dead battery flag but i do not see it even set.