Part Number: P82B96
We intend to use the P82B96 to extend I2C interfaces. VCC will be 12V. The master interface is a TIVA processor with only 3.3V compatible I/O. Will the SY and SX interfaces be compatible with the TIVA? I don't see voltage levels for the RX and RY outputs described (when data is sent to the TIVA). However, I see that the master interface is compatible with 3.3V pullups. Thanks!