Part Number: DP83TG720S-Q1
HI SIR
Could I use below structure?
as below, RJ45 will connect to our computer, and Automotive MATEnet will connect to DUT on the other side

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TG720S-Q1
HI SIR
Could I use below structure?
as below, RJ45 will connect to our computer, and Automotive MATEnet will connect to DUT on the other side

Hello Chen Alex 1,
Thank you for the query.
Are you asking if you can do this on the EVM or the board you design.
You should be able to do this on the board that you design.
Regards,
Sreenivasa
HI SIR
if you have any guide for direct comm without MCU,as you know, now mcu is out of stock
Hello Chen Alex 1,
Thank you for the reply.
I am not able to understand you reply. Is this a custom board or EVM ? If it is EVM, the MCU is on the board.
Regards,
Sreenivasa
Hello Chen Alex 1,
I am not able to understand you reply. Is this a custom board or EVM ? If it is EVM, the MCU is on the board.
Regards,
Sreenivasa
I mean, if I can I use DP83867 & DP83TG720 direct comm without MCU In the deisgn?
thanks
Hello Chen Alex 1,
Thank you for the reply.
This should be fine in the design, If you do not have additional question, please click the resolved button to close the thread.
Regards,
Sreenivasa
Hello Chen Alex 1,
Is the deign in planning or complete?
Regards,
Sreenivasa
Hello Alex1,
Thank you for the update.
We can support with the review when the design is ready for review.
If you do not have additional questions, please click the resolved button to close.
Regards,
Sreenivasa