Part Number: TUSB320LAI
Other Parts Discussed in Thread: TUSB320
Hello,
I wonder if the TUSB320xAI can be used with different currents for sink/source mode. The circuit will have a non-USB power supply as primary source. When using this supply, the USB port shall provide 5V/500mA (USB 2.0). If the main power supply is not available and a USB power supply is used, the port draws 5V/3A. Is this possible with TUSB320xAI devices?
If it's possible, I'm still not sure if I understood all TUSB320xAI modes correctly:
1) Which mode has to be used, DRP or DFP with dead battery?
2) For the above, I²C mode must be used, right?
Regards