Part Number: DP83867IR
Hi team,
When they use DP83867IR at 100Mbps & RGMII, should they use TD_P_A、TD_M_A and TD_P_B、TD_M_B as MDI ports?
Regards,
Noriyuki Takahashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IR
Hi team,
When they use DP83867IR at 100Mbps & RGMII, should they use TD_P_A、TD_M_A and TD_P_B、TD_M_B as MDI ports?
Regards,
Noriyuki Takahashi
Thank you for the query. Please refer below
Regards,
Sreenivasa
Sreenivasa,
It seems TD_P_A、TD_M_A and TD_P_B、TD_M_B work as both transmitter and receiver. In case of DP83867IR at 100Mbps & RGMII, those pins work as below?
TD_P_A: Receiver +
TD_M_A : Receiver-
TD_P_B: Transmitter+
TD_M_B: Transmitter-
Regards,
Noriyuki Takahashi
Hello Noriyuki Takahashi
Thank you for the reply.
Yes, your understanding is correct.
Regards,
Sreenivasa
Hello Noriyuki Takahashi
The below thread could be used as reference.
Regards,
sreenivasa
Hi Sreenivasa,
You mentioned the below is correct, but it seems TD_P_A and TD_M_A work as transmitter based on the
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1005225/dp83867is-100-base-tx-mode-tx-and-rx-pins/3716400. Which is correct?
TD_P_A: Receiver +
TD_M_A : Receiver-
TD_P_B: Transmitter+
TD_M_B: Transmitter-
They also have several questions.
- In the post, we can see the comment as below. Does this mean that they don't need to care about TD_P_A works as receiver or transmitter?
"But if using auto-mdix, each pair can function as either RX or TX."
Regards,
Noriyuki Takahashi
Hello Noriyuki Takahashi
The below would help you understand batter.
8.4.3.9 Auto-MDIX Resolution
The DP83867 can determine if a straight or crossover cable is used to connect to the link partner. It can automatically re-assign channel A and B to establish link with the link partner, (and channel C and D in 1000BASE-T mode). Auto-MDIX resolution precedes the actual Auto-Negotiation process that involves exchange of FLPs to advertise capabilities. Automatic MDI/MDIX is described in IEEE 802.3 Clause 40, section 40.8.2. It is not a required implementation for 10BASE-Te and 100BASE-TX.
Auto-MDIX can be enabled or disabled by register configuration, using bit 6 of the PHYCR register (address 0x0010). When Auto-MDIX is disabled, the PMA is forced to either MDI (straight) or MDIX (crossed). Manual configuration of MDI or MDIX can also be accomplished by register configuration, using bit 5 of the PHYCR register. For 10/100, Auto-MDIX is independent of Auto-Negotiation. Auto-MDIX works in both Auto-Negotiation mode and manual forced speed mode.
0X0010
MDI Crosssover Mode:
1x = Enable automatic crossover
01 = Manual MDI-X configuration
00 = Manual MDI configuration
Regards,
Sreenivasa
Sreenivasa,
How about the question as below?
You mentioned the below is correct, but it seems TD_P_A and TD_M_A work as transmitter based on the
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1005225/dp83867is-100-base-tx-mode-tx-and-rx-pins/3716400. Which is correct?
Regards,
Noriyuki Takahashi
Hello Noriyuki Takahashi
The default is 1x = Enable automatic crossover. So both are correct.
If you set to 00 = Manual MDI configuration TD_P_A and TD_M_A work as transmitter
Regards,
Sreenivasa