Part Number: TPS65988
Other Parts Discussed in Thread: HD3SS3202,
Hi Team,
Would you share your mailing list for sending email because I would like to ask questions with our confidential information?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yoshifumi,
Please see my comments below.
1. C11 should be 2.2uF min, 4.7uF typ and 6uF max.
2. Recommend adding a bypass cap with 5uF min, 10uF typ.
3. Recommend adding a bypass cap with 47uF typ, 120uF max.
4. Recommend adding 10nF caps on each Vbus pins (A4, B4, A9, B9) at the Type C connector.
Please reach out to the HD3SS3202 group to review that portion. Thanks.
Best regards,
Penny
All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).
Hi Yoshifumi,
Sorry for missing that information in my previous reply,
2. Recommend adding a bypass cap between VIN_3V3 (pin 5 of TPS65988) and ground with 5uF min, 10uF typ.
3. Recommend adding a bypass cap between PP_HV1(pin 11,12) /PP_HV2 (pin 1, 2) and ground with 47uF typ, 120uF max.
Hi,Penny
Thank you for checking.
I want to reduce the mounting area.
If "Multiport Sink Policy" is set to "Only highest power sink path closes switch",
is it okay to delete the circuit in the blue frame?
Regards
Hi Yoshifumi,
You can simplify the design if your configuration only enables the power path with the highest power PD contract.
Please see this section in datasheet: