Part Number: THVD1500
Hi,
We are using THVD1500 at 5V. The board is powered using 5V over a connector and we have added a 5V TVS diode at the connector.
The clamping voltage of the TVS diode is around 9.2V whereas the absolute maximum rating of VCC pin is 7V.
Would this cause an issue (potentially damaging the transceiver) or it is fine since it is a momentary surge pulse?