Part Number: TPS65988DK
Other Parts Discussed in Thread: TPS65988,
Hello,
We are using two different hardwares in spi less mode, in configuration 5 (with ADCIN1 = 1, not in dead battery mode):
a. The TPS65988DH chip on the TPS65988EVM board (DeviceInfo = "TPS65988 HW0030 FWF707.10.00 ZAce1")
b. A home made board (same power path design than EVM) but with a TPS65988DK version (DeviceInfo = "TPS65988 HW0030 FWF907.14.00 ZAce1")
Our host controller (stm32) is writing its configration as a DRP (same issue as UFP), configuration created with customization tool templates.
With the same host code (so same TPS configuration), the 'a' hardware is switching correctly corresponding PP3 or PP4 external switch, BUT on the 'b' hardware, no outputs are driven (whereas the PP3switch or PP4switch fields of the"power path" register are set to 3 as "switch enabled (system input). GPIO set logic high.").
We are not applying any patch, just writing configuration over i2c after "mode" register read to "APP".
So my question, is there any behavior differences between DK and DH series concerning exteral switches ?
Or is it linked to the default ROM FWF version ?
Or is there something wrong in our method ?
Thanks in advance for your answers.