Part Number: TSB12LV32
Other Parts Discussed in Thread: TSB81BA3E, TSB82AA2, TSB82AA2B, XIO2213B
Hi sir,
I have an internal study of the application to acquire commands from the host device via IEEE1394b and to control it.
Specifically, the transmission is performed by the TSB81BA3E, the transceiver of IEEE1394b, and the data is converted by the LLC of "TSB12LV32" , and read and control data in DSP「TMS320F2833x」.
I have the queries as below.
1. Is there any problem with the above device selection? If there is a problem, can you propose an alternative?
The data sheet of "TSB12LV32" corresponds to IEEE1394a , but can it be used for IEEE1394b?
2. If I read data from two DSPs, is it possible to connect multiple DSPs to "tsb12lv32"?
3. Could you suggest any information related to IEEE1394b (Evaluation Kit, etc.)?
Thank you for your suggeston.
Regards,