This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
May I have a question for DP83867IR RGMII signal Voltage.
DP83867RRGZ has RGMII interface.
Question1. How much the signal voltage spec Rx,Tx(Voh/Vol,Vih,Vil) in RGMII?
Question2. Does it same spec with clock and Data?
BR,
Kosaka
Question3. There is RGMII signal spec in "7.9 RGMII Timing" RGMII is 2.5V interface.
And there is some criteria TskewT,TskewR etc.
How much voltages should we check the skew?
BR,
Kosaka
Hi Kosaka-san,
RGMII is dependent on the VDDIO level. The logic levels of this would be located in section 7.5 in the datasheet. Clock and MAC data should be under VDDIO domain. For skew, the times should be measured at 50% of VDDIO level.
Sincerely,
Gerome