Part Number: XIO2001
Hello,
I'm trying to connect XIO2001 and PCI Device IC directly, but I don't know how long the Address / Data line should be.
Is there a regulation regarding the length of the Address / Data line in XIO2001?
M.UEDA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XIO2001
Hello,
I'm trying to connect XIO2001 and PCI Device IC directly, but I don't know how long the Address / Data line should be.
Is there a regulation regarding the length of the Address / Data line in XIO2001?
M.UEDA.
Thank you for your reply Nasser
Thanks to that, one question was solved.
As an additional question, do all Address / Data lines from 0 to 31 have to be the same length?
I'm sorry for all the amateur questions, but please answer.
M.UEDA.
The datasheet says:
All synchronous PCI bus signals must be length matched to meet clock setup and hold requirements.
Also see section 9.3.1.