This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1297: Signal loss due to pathological signal on the LMH1297EVM

Part Number: LMH1297


We are facing signal loss when 12G pathological signals are used with TI LMH1297EVM.

Signal loss occurs once every 2-3 hours in EQ mode. 

No signal loss has occurred with the colorbar signal. 

I think it's due to the out of sync of the CDR.

Do you have any idea to solve this problem?

The conditions of the evaluation  as follows 

Signal Generator : FOR A ESG-4100

Multi Waveform Monitor : LEADER LV 5400

SDI_IO Input Cable : CANARE L5.5CUHD

Length  2m EQ_GAIN Value : 3

             3m EQ_GAIN Value : 3

           30m EQ_GAIN Value : 9

             All No Signal occurs 

OUTPUT : OUT0

                  SDI_OUT

             All No Signal occurs 

Rerards, 

H.Okada