Part Number: TPS25750
Other Parts Discussed in Thread: BQ25731, BQ25790, BQ25792, USB-PD-CHG-EVM-01, TIDA-050047,
Hi team,
Our conditions are the following.
Then, we would like to know a recommended Battery charger and have two questions.
[Our conditions]
-Sink only
-Around 65W (Voltage and current are TBD)
-4cell Battery
-----------
[Q1]
I found the following comment in TI HP and understand that if 65W, a recommended Battery charger is BQ25731.
Why is 45W the threshold?
And, can't I use BQ25792 or BQ25790?
If yes, could you please let us know the reason?
<TI HP>

-----------
[Q2]
I would like to use USB-PD-CHG-EVM-01(TPS25750D + BQ25792).
I understand that EVM can sink 100W(20V/5A) so can use BQ25792 for 65W.
Is my understanding correct?
If yes, I would like to use BQ25792 for 65W.
Could you please let us know if you have any concern?
< Design Guide: TIDA-050047>

-----------
Regards,
Hide