Part Number: DS250DF230
1. In Our design we are using two DS250DF230. Is it possible to provide a SPICE model for TINA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF230
1. In Our design we are using two DS250DF230. Is it possible to provide a SPICE model for TINA?
We are using this in the SFP28 where we will receive PTP + SYCNE.
Due to high trace length (500mm) we are using active cable method implementation in PCB itself ( two retimer per TX and two retimer per RX channel)
From the datasheet, I understand that <500ps latency will be there per retimer , Since we are having two retimer. I am expecting 1nS latency.
Since ours is a PTP steered system. We should expect this 1nS time delay in our PTP? or some more latency will also get added?
Note:- retimer reference 30.72 Mhz is provided by the separate oscillator. this will not be in sync with the PTP
(is this an issue ? do we need to steer the retimer reference clock as well as be ptp steered ?)
The maximum copper trace length depends on the dielectric material used and channel performance. The retimer Rx EQ (DFE + CTLE) can typically compensate up to 35dB of insertion loss at 25Gbps.
You may request download access to the DS250DF230 IBIS-AMI model files via the TI.com product page. See link below.
https://www.ti.com/drr/opn/DS250DF230-DESIGN
Thanks,
Rodrigo Natal
thanks rodrigo,
" We are using this in the SFP28 where we will receive PTP + SYCNE.
Due to high trace length (500mm) we are using active cable method implementation in PCB itself ( two retimer per TX and two retimer per RX channel)
From the datasheet, I understand that <500ps latency will be there per retimer , Since we are having two retimer. I am expecting 1nS latency.
Since ours is a PTP steered system. We should expect this 1nS time delay in our PTP? or some more latency will also get added?
Note:- retimer reference 30.72 Mhz is provided by the separate oscillator. this will not be in sync with the PTP
(is this an issue ? do we need to steer the retimer reference clock as well as be ptp steered ?) "
Please provide details for this query as well. If this is not clear please let me know
See my inputs below.
From the datasheet, I understand that <500ps latency will be there per retimer , Since we are having two retimer. I am expecting 1nS latency. Since ours is a PTP steered system. We should expect this 1nS time delay in our PTP? or some more latency will also get added?
Retimer reference 30.72 Mhz is provided by the separate oscillator. this will not be in sync with the PTP. Is this an issue ?
This is not an issue. The 30.72MHz calibration clock does not actually feed into the data path. it is mainly used by the retimer digital logic to serve as reference for the PPM check function. Each retimer channel will recover the clock from the input data and then this recovered clock serves as reference to the sampler.
Regards,
Rodrigo
Due to high trace length (500mm) we are using active cable method implementation in PCB itself ( two retimer per TX and two retimer per RX channel)
As mentioned earlier we are using the active cable method in PCB, Currently, we are using one oscillator cascaded to all four retimer with the help of CAL_CLK_OUT.
In this way, we need to route the lvcmos clock also along with high-speed signal.
Can we have two seperate clocks for each retimer pair? as mentioned in the image. will this affect the system in any way?
Due to high trace length (500mm) we are using active cable method implementation in PCB itself ( two retimer per TX and two retimer per RX channel)As mentioned earlier we are using the active cable method in PCB, Currently, we are using one oscillator cascaded to all four retimer with the help of CAL_CLK_OUT.
In this way, we need to route the lvcmos clock also along with high-speed signal.
Can we have two seperate clocks for each retimer pair? as mentioned in the image. will this affect the system in any way?
Please help us in this,
Can you please verify our SCH if I have made any mistake in the 4 retimer solution in SFP?
Regarding: "Can we have two seperate clocks for each retimer pair? as mentioned in the image. will this affect the system in any way?"
Schematic inputs below. No problem identified, just a comment on the high-speed I/O AC coupling caps.
Checked and ok
Comment