Part Number: TPS6598X-CONFIG
Hi. I need to download some customer legacy design bit files and using the latest GUI build V6.1.2 fails to program and verify the Flash SPI PROM. The project file reports build version of 6.1.1 and we cannot rebuild it to 6.1.2, nor do we have access to the machine on which the 6.1.1 GUI tool was installed, so we need a loadable copy of the V6.1.1 GUI config tool. TI does not seem to have a download archive (bad idea), and Wayback Machine saved the link page to 6.1.1 but didn't save the actual download link/file as the GUI tool download requires authorization.