Part Number: DP83848VYB
Hello all,
I have an issue regarding ethernet with esp32, So i have got designed a hardware with esp32 and dp83848 phy for ethernet connection. The problem is i dont get Link Up from phy. I am running esp32 [example code](github.com/.../basic) PHY reset pin is 32. this is log output from board, it just stops at Ethernet started,
V (2958) tcpip\_adapter: check: local, if=2 fn=0x400e24d8 \[0m V (2958) tcpip\_adapter: call api in lwip: ret=0x0, give sem\[0m V (2958) tcpip\_adapter: check: remote, if=2 fn=0x400e24d8 \[0m D (2968) event: running post ETH\_EVENT:0 with handler 0x400d3a84 on loop 0x3ffb4f7c\[0m \[0;32mI (2978) eth\_example: Ethernet Started\[0m
I checked the communication between phy and esp32, this sounds good, as i tried to read phy register and below was output, i had used [cyclone TCP](www.oryx-embedded.com/.../CycloneTCP) example code for this., so this conclude phy and esp32 are communicating,
>Initializing DP83848... > >PHY reg: 00: 0x3100 > >PHY reg: 01: 0x7849 > >PHY reg: 02: 0x2000 > >PHY reg: 03: 0x5C90 (this is phy address) > >PHY reg: 04: 0x01E1 > >PHY reg: 05: 0x0000 > >PHY reg: 06: 0x0004 > >PHY reg: 07: 0x2001 > >PHY reg: 08: 0x0000 > >PHY reg: 09: 0x0000 > >PHY reg: 10: 0x0000 > >PHY reg: 11: 0x0000 > >PHY reg: 12: 0x0000 > >PHY reg: 13: 0x0000 > >PHY reg: 14: 0x0000 > >PHY reg: 15: 0x0000 > >PHY reg: 16: 0x0000 > >PHY reg: 17: 0x0000 > >PHY reg: 18: 0x0000 > >PHY reg: 19: 0x0000 > >PHY reg: 20: 0x0000 > >PHY reg: 21: 0x0000 > >PHY reg: 22: 0x0100 > >PHY reg: 23: 0x0021 > >PHY reg: 24: 0x0000 > >PHY reg: 25: 0x8021 > >PHY reg: 26: 0x0904 > >PHY reg: 27: 0x0000 > >PHY reg: 28: 0x0000 > >PHY reg: 29: 0x6011 > >PHY reg: 30: 0x003F > >PHY reg: 31: 0x0000
so now i have to check between RJ45 jack and PHY, i actually dont understand what is the issue, but i am sure its between phy and RJ45 jack,
i have tried the connection with router and PC directly, also tried using different LAN cable, but didnt work
From forum, i checked PFBout, it is 1.75v,
Here's Schema: https://imgur.com/a/W36Dv9Z
So any help regarding this will be grateful if any more information is needed kindly tell me.
PCB Layout :