Part Number: DP83TD510E
Hello,
I want to use straps to configure the DP83TD510E in RMII Slave mode, but it is not clear to me from the datasheet how to do that and support the LED_0 functionality on pin 29. I understand I need to strap pin 29 (LED_0) high, but now I need to attach the LED to pin 29.
LED_0 is active low by default (per LEDS_CFG_2 Register (Address = 0x469)).
So I believe I need a 2.49K pullup on pin 29 in parallel with my LED and a current limiting resistor - like this:

Do I have it correct?
Thanks,
Cyrus