Part Number: DS90UB948-Q1
Hi Team,
There is a good new that we DIN DS90UB948-Q1
And there have one thing need your support!
Please help check this SCH, THX
At present, the PASS and LOCK lights of UB948 power transmission test are off (connect to UB941)
The circuit is shown in the figure. The currently measured PDB pin is 3.3V.
Does the UB948 SCH need to be adjusted?
The current measurement C6=0V & C7=C34=2.5V! There seems to be a problem with UB948 now