This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: discrete components around TUSB9261

Part Number: TUSB9261

Hi Team,

My customer is designing their board with TUSB9261 now and I got some questions about some discrete parts around TUSB9261.
Could you help me to answer their questions following?

1. Regarding "2.8 USB VBUS" in TUSB9261 Implementation Guide(SLLA315E), it says that 5V should be divided by 90.9K and 10k ohm register with 1% accuracy. They want to use 91kohm resister instead of  90.9K one but Is it acceptable for the device?
2. Could you tell me how they deal with USB3.0 pins if they don't plan to use the high speed pins? They plan to use only USB2.0 lines.

Regards,

Takashi On