Part Number: TUSB4020BI
Hi,
I do not use the pins whose names I have written below.
What I should do when I do not use these pins is not specified in the pin table in the datasheet.
What should I do with these pins?
PWRCTL1/BATEN1 *I use the downstream port1 for USB communication, but I don't need these pins because I don't use a power switch.
OVERCUR1z *I use the downstream port1 for USB communication, but I don't need these pins because I don't use a power switch.
SMBUSz *I will not use SMBUS or I2C.